Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide12

The slave side of the ANT connection needs to establish a link with the master. In order to do this effectively on a coin cell battery the receive radio is turned on and off by ANT. This patented search algorithm uses about a 10% duty cycle, meaning that the radio is actually off for over 90% of the time. Since there is no master clock in an ANT network a slave has no idea of when a master will transmit, so the search algorithm varies the receive window spacing and usually connects within four message periods. Since the radio is used much more in search mode, to save battery capacity care must be taken in turning the search off when no master has been found. An ANT search takes an average power of about 3mA vs. average powers of less than 25µA for a synchronized ANT message.

PTM פורסם ב: