Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 12

The buck regulator has two different states, when switch S is closed and when switch S is open. When the switch is closed, current from VIN charges flow through the inductor, charges the capacitor, and supplies the output load current. When the switch is open, the magnetic field in the inductor collapses and causes the voltage across the inductor to change polarity. This change in polarity pulls the phase node below ground, forward biasing the diode. This allows current to continue to flow as the inductor sources the current needed by the load.

PTM פורסם ב: