Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 18

For a stable system, the gain must be less than one by the time a 360o phase shift occurs. The error amplifier inverts the signal (180o phase shift); added to the 180o phase shift of the L-C filter results in a 360o phase shift. If there is gain at the L-C corner frequency, a voltage mode converter will oscillate. For voltage and current mode controllers, compensation is required to get the adequate phase and gain margins required for stability. Designers should keep in mind that the desired phase margin is 45 - 60°. Compensation can be fixed internally (minimizes external components but limits choice of output filters).

PTM פורסם ב: