Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 16

The duty cycle for a buck regulator is defined as the ratio of tON to T. The output voltage is set by multiplying the input voltage by duty cycle. The amount of ripple current is also calculated by using duty cycle. As can be seen, the amount of ripple is proportional to duty cycle, the length of the total cycle time, and the difference between VIN and VOUT. It is inversely proportional to the amount of inductance in the system. Ripple current is used to calculate how much ripple voltage will be seen at the output. Ripple voltage is calculated by multiplying the ripple current by the ESR of the output capacitor.

PTM פורסם ב: