Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 22

The voltage mode controller is a very well understood topology and it has a constant frequency, which are big advantages. However, the inductor and capacitor of the power stage form a double-pole filter and is hard to compensate. The compensation takes many components to achieve properly. In addition, due to the architecture of a voltage mode controller, COUT may have to be large to get acceptable transient performance.

PTM פורסם ב: