Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 17

Gain margin is the gain of magnitude when phase reaches 180°. Phase margin is defined as the amount of phase above 180° when the loop gain crosses 0dB. The higher the phase margin, the more stable the system. The preferred phase margin is greater than 45°. The two blocks shown are commonly referred to as the modulator and the power stage. Together, they form the bode plot shown. The gain margin for the plot is 18dB while the phase margin is 15°. With a preferred phase margin of 45° or more, something must be done.

PTM פורסם ב: