Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 24

The unique control architecture from Semtech shown here is referred to as “Adaptive ON-Time” control. This control does not use an error amp and hence provides extremely fast loop and transient response. It uses ripple voltage to trigger the on-time of the controller. The adaptive on-time is determined by an internal one-shot timer as shown. When the one-shot timer has been triggered by the output ripple, the device sends a single on-time pulse to the high-side MOSFET. This pulse period is determined by VOUT and VIN. The period is proportional to the output voltage and inversely proportional to input voltage. This arrangement automatically anticipates the on-time required to regulate VOUT for the present VIN and at the selected switching frequency.

PTM פורסם ב: