Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 9

In this example, VIN has been defined as 3.3V, VOUT as 2.5V, and 10kΩ selected for R2. From the equation for calculating R1 and using the value of 0.5V for VREF from the datasheet, a value of 40kΩ is needed for R1. TAMBIENT is also defined to be 50 °C. From the datasheet, TJ-MAX is calculated as 125 °C, and RTHETA-JA defined as 36 °C/W. With those values, the maximum available output current will be 2.6A.

PTM פורסם ב: