Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 4

TJ-MAX is the highest allowable temperature the junction in the IC is allowed to achieve. TA is defined as the ambient temperature of the air in the vicinity of the regulator. RTHETA-JA is the thermal resistance from the junction to ambient. This includes the thermal resistance from the junction-to-case, the case-to-PCB, and PCB-to-air. VFB is the feedback voltage used to set the output voltage. R1 and R2 create a resistor divider to form VFB from VOUT. The error amp works to keep VFB equal to VREF.

PTM פורסם ב: