Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 29

First, calculate the TON time from the equation shown in this slide. Use the maximum VIN value for the TON calculation. For these parameters, a TON time of 318ns is calculated. An equation for calculating the resistor for setting RTON can be found on the SC417 datasheet. For this example a value of 154.9kΩ is calculated. The closest 1% value of resistor is 154kΩ. To set the output voltage, use the previously presented feedback equation. From this, select 10kΩ for RFB2 and 11kΩ for RFB1. To calculate the ripple current, use the equation found on slide 16 which includes the terms D and T. For D, use VOUT/VIN max and for T, use 1/FSW. Ripple current is then calculated to be 3.9A peak-to-peak.

PTM פורסם ב: