Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 19

These charts show the impact of adding compensation. The previous bode plot has shown that the phase margin is 15°. As mentioned on the previous slide, the error amplifier shown will cause a 180° phase shift, but is not shown in the plot. Z1 and Z2 form the compensation, which can be seen in the closed loop response plot, to improve the phase margin to over 60°.

PTM פורסם ב: