Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 30

To stay under the VRIPPLE requirement of 30mV, an ESR value of under 7.7mΩ is needed. By using two 220μF capacitors with 15mΩ of ESR each, an ESR of 7.5mΩ will keep the VRIPPLE within requirements. The final component value to calculate is RILIM. This is done by using the equation listed and is calculated as 7.35kΩ. A 7.5kΩ value can be used to maintain a 10A current limit.

PTM פורסם ב: