Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 28

For a constant on-time regulator with integrated FETs, the SC417 will be examined. This design will use the following parameters: VIN will equal 12V, VOUT equals 1.05V, IOUT equals 10A, the desired switching frequency is 250kHz, and the output voltage ripple needs to be under 30mV.

PTM פורסם ב: