Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 13

On the previous slide, it was shown that the diode becomes forward biased with the collapsing of the magnetic field of the inductor. This occurs without any reference to a clock and hence is known as an asynchronous regulator. The VF of the diode used represents a significant portion of losses within an asynchronous regulator, especially as the value of VF approaches the value of VOUT. By replacing the diode with another MOSFET, the losses in the system can be reduced. This requires a more complex controller to ensure the MOSFETs are not both turned on at the same time. Since the bottom MOSFET is now controlled, the topology is referred to as a synchronous regulator. In the schematic on the right, S1 is referred to as the top FET or the high-side FET while S2 is referred to as the bottom FET or the low-side FET.

PTM פורסם ב: