Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 8

Linear regulators can be classified as either integrated or discrete. An integrated linear regulator has the pass element integrated in the package. A discrete solution has an external pass element. Feedback components may or may not be integrated for either a discrete or integrated regulator. The SC339 is an example of a discrete linear regulator, while the SC4215H is an example of an integrated linear regulator.

PTM פורסם ב: