Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 23

A current mode control has many advantages including an excellent output voltage regulation. Due to the architecture, the inductor is turned into a current source. With the inductor as a current source, the capacitor on the output has a single pole filter effect. This makes the loop easier to compensate than the voltage mode controller. Since current is part of the loop, current limiting is built in. There are disadvantages to using a current mode controller. For one, the transient response is slower when compared to a constant on-time regulator. Also, the current signal is often a very small value and any noise induced in the system can affect regulation.

PTM פורסם ב: