Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 33

The SC189 is a voltage mode controller that allows up to 1.5A of output current. Compensation for the controller is handled internal to the part. The SC189 comes in eleven fixed output voltage varieties. Since the compensation is internal, specific components are required to maintain stability. Which components are required depends on the output voltage required. The table on this page shows the required components for voltage outputs less than or equal to 1.5V.

PTM פורסם ב: